Hi Team,
Our customer would like to clarify about the input impedance of TRF370417. According to our customer,
I'm using a couple of TRF370417 mixers in my design. In table 6.5 on page 5 of the data sheet it says that ZI(single ended) has an "input impedance, resistance" of 5 KOhms and an input impedance, parallel capacitance of 3 pF. So, is that saying that the port input impedance is not 50 Ohms? Also, in 8.1.1 on page 18 a bullet says "Terminate the ac-coupled LON with 50 ohms to GND. Does this mean hang a resistor on that port? What about LOP??? Isn't this port 50 Ohms??? How come your reference design shown in Figure 44 on page 19 don't have any of this? Which ports, if any, on this device that are NOT 50 Ohms across the specified operating band of the device?
Regards,
Danilo