This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CELLIN is considering designing a DPD PA module with the following configurations using the AFE7686.
Please advise configuration for this mode
For:
- REF_CLK = 368.64MHz
- ADC sample rate = 2949.12MHz, DEC = 4, Data interface = 737.28MHz
- DAC sample rate = 8847.36MHz, INT = 12, Data interface = 737.28MHz
- JESD204B N’=12 / TX = 11.0592Gbps / RX = 11.0592Gbps
- 4T4R RF frequency = 3.84GHz TDD
Please see below for configuration:
The customer has further inquiries.
1. They want to change the serdes lane settings as below. Could you please provide a sample configuration file?
2. According to the AFE7686 datasheet below, the SCLK for Temperature sensor read is typical 1uS.
Is it okay to use 10MHz or higher as the SCLK for Temperature sensor read?
Regarding
- REF_CLK = 368.64MHz
- ADC sample rate = 2949.12MHz, DEC = 4, Data interface = 737.28MHz
- DAC sample rate = 8847.36MHz, INT = 12, Data interface = 737.28MHz
- JESD204B N’=16 / TX = 14.7456Gbps / RX = 14.7456Gbps
- 4T4R RF frequency = 3.84GHz TDD
Please see configuration file below:
CellinAFE7686_44210Mode_14p74Gbps.cfg
Regarding
According to the AFE7686 datasheet below, the SCLK for Temperature sensor read is typical 1uS.
Is it okay to use 10MHz or higher as the SCLK for Temperature sensor read?
This will impact the accuracy of the temperature sensor reading and we cannot ensure the correct operation.
-Kang