Other Parts Discussed in Thread: AFE7900
I have a custom board design with AFE7900 and Xilinx Xcku050 FPGA.
I want to test my JESD lanes with registers B7h (DAC JESD - TX_JESD_TEST_S IG_GEN_MODE ) and 108h, 109h (ADC JESD - RX1_JESD_TEST_SIG_GEN_MODE, RX2_JESD_TEST_SIG_GEN_MODE) by sending ramp signals. (I am sending this commands both AB and CD pages of AFE).
1) When I write the value 0x2 to the B7h register, I can see the Ramp signal from the FPGA, but when I disable the B7h register and apply an external signal to the AFE, I can only see the noise in the FPGA.
Will this test fully verify my JESD connection at TX side and what could be the cause of this Issue ?
2) When I write the value 0x2 to the 108h and 109h registers, I can verify with the spectrum analyzer that the Ramp signal comes out of the AFE, but there is no signal from all the AFEs on my board and I see the signal corrupted in some of them? (Also, I have checked this tests with my EVM and I know what is the output of AFE with same configurations)
Will this test fully verify my JESD connection at RX side and what could be the cause of this Issue ?
I need help on this problem?
Thanks in advance.