Part Number: AFE7950
Hi,
The application I am developing is radar system. I think that FB channels are not needed and TDD mode is enabled.
1> How can I disable FB channel in Latte script file?
After disabling FB, RRFMode 5 and 6 operate equally for TDD mode?
2> sysParams.serdesFirmware should be 'True' ?
If this param is set to 'True', which firmware would be downloaded? Where can I see the serdesFirmware source?
3> AFE.systemStatus.loadTrims should be '1'?
4> sysParams.topLevelSystemMode
Where can I find the description about topLevelSystemMode.
Regards,
YS