Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950, LMK04832
Hi Team,
I wanted to check with you how is the external clock (e.g. 163.68 MHz) provided to the AFE7950EVM on connector J14 distributed throughout the evaluation board.
I understand that AFE7950 system clock lane will be necessary (from which e.g. ADC and DAC sampling rates will be derived), but also there is the LMK that sends multiple outputs, some of which are going towards the FPGA (in this setup FPGA is connected to the AFE eval. module).
Does the LMK take as input the external clock and then provide all the necessary clock outputs to both AFE and FPGA, or is there any additional clock signal splitting happening on the eval board?
In addition, is the same clocking distribution then applied to the AFE7950 device in standalone mode (without eval board that comes with extra LMK and other components), given that the user provides dedicated LMK device?
Kind regards,
Željko