This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950: The DAC output power is small, which affects chip evaluation

Part Number: AFE7950
Other Parts Discussed in Thread: AFE7900EVM,

The DAC output power is small, which affects chip evaluation

For example, the planned output frequency of a single carrier signal is 1500M, and the measured signal power at 1500MHz is only -25dBm, while the DAC reference clock frequency and 1500MHz cross-modulated signal is still large, about -13dBm, so it feels that the DAC is the mix mode of Zone 2 Nyquist. So earlier I wanted to ask latte if Latte has an instruction set that configurates the chip to a zone 1 Nyquist working mode