For programming the the NCO frequency, 16 bit frequency word can be programmed via SPI. I want to know the time after which ti will reflect, and the constraints it puts on the maximum hopping rate from one frequency to another.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For programming the the NCO frequency, 16 bit frequency word can be programmed via SPI. I want to know the time after which ti will reflect, and the constraints it puts on the maximum hopping rate from one frequency to another.
Hi AK,
To program the NCO through SPI there are a series of register writes that must be performed, see sequence below. This means that when switching by SPI you will be limited by the amount of time it takes to perform the SPI writes mentioned below. One thing to note is that if your application allows you to know the next frequency ahead of time then you can load the 32 bit word and wait to toggle the NCO load bit till it is required.
1. Open the Rx/Tx Dig Page (1 SPI write)
2. Write the 32 bit word (4 SPI writes)
3. Set the NCO load bit to 1 (1 SPI write) [NCO is loaded only when this bit is toggled from 0 to 1]
4. Set the NCO load bit to 0 (1 SPI write) [Toggle bit back to 0 for next NCO load]
4. Close the Rx/Tx Dig Page.
Regards,
David Chaparro