Other Parts Discussed in Thread: AFE7900EVM, AFE7900,
Hi,
I would like to inquire about the matching network configuration of AFE7950 inputs and outputs.
- The DAC output frequency to be used is from 3.25GHz to 3.75 GHz.
Can you provide a matching network suitable for the dac output frequency ?
2. The DAC output frequency to be used is from 0.8GHz to 1.3 GHz
Can you provide a matching network suitable for the dac output frequency ?
3. The ADC & FB input frequency to be used is from 2.4GHz to 2.5GHz.
Can you provide a matching network suitable for the ADC & FB input frequency ?
4. What is the frequency band of the matching network applied to ADC and DAC in the AFE7900EVM_DesignFile (DC135A_AFE7900EVM_Sch.pdf)?
Please let me know by TX/RX/FB channel.
5. Can you provide a matching network used in the different bands shown on page 20 of the afe7950 datasheet?
Thanks.