This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: Xilinx boad user interface for reference design based on ZC706 Xilinx board

Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950,

Hi Team,

I noticed that for ZCU102 Xilinx board in your reference design there is software with an option to change the value of Vadj voltage.

Since in our work we've been using AFE7950EVM with ZC706 eval kit (as per TI reference design), we wanted to enable external SPI programming of the AFE7950.

However, we've learned that ZC706 eval kit has different voltage (Vadj = 2.5V) over the relevant SPI lines going through the FMC when compared to the AFE EVM (1.8 V). So, I wanted to know can the Vadj voltage be adjusted somehow programmatically on ZC706 or we will have to physically modify the electrical path of the SPI lines.

Kind regards,

Željko