Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950
Hi Team,
We've been looking into using an FPGA (ZC706, as per TI reference design) to program the AFE7950EVM over the SPI lines. For this process, two major components need to be programmed:
- AFE7950
- LMK on the EVM
As far as I understand the AFE7950 EVM should be fairly straightforward to program as there are some SPI lines going from it to the FMC on the EVM. However, the LMK, if I understand correctly, is being programmed solely via the USB connection with PC (and Latte) and there are no dedicated LMK SPI lines going to the FMC. Can you confirm if this is the case, and if so, could you suggest some measures that can be taken to connect LMK with FPGA through SPI lines?
Kind regards,
Željko