Other Parts Discussed in Thread: AFE8000,
Hello,
I am trying to bring up the AFE8000 EVM.
My environment is below.
FPGA Board : ZCU102
Connector used : HPC1
SW : Latte (AFE80xxCat)
10MHz ref : not connected.
To quick review, I first loaded an excel file in Latte.
The file name is "AFE80xx_SystemParameters_2949p12_8847p36_RX_245p76p64_TXFB_491p52.xlsx"
In this configuration file, Fref is 491.52MHz. After I checked the real frequency value
(measured it by connecting two wires on resistors R326 / R331 in the schematic),
frequency seems not to properly set. The measured value was about 500MHz.
Also, in the top page of AFE80xx sw, when I changed the FPGA input clock value
250 to 245.76MHz the value is not changed.
(measured the frequency value by connecting two wires on resistors C339 / C340 in the schematic)
125MHz is well applied and changed.
Here, what I want to know is that "Can't I change the frequency value to the multiples of 122.88MHz in the latte software?"
Do I have to control LMK using fpga through the FMC connector?
Thanks in advance.