Hi Experts,
I have a customer that is asking for a device Direct Digital Synthesizer that can chirp 0-2 GHz in <10us. I am just wondering if we have that kind of device.
Your response is highly appreciated. Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts,
I have a customer that is asking for a device Direct Digital Synthesizer that can chirp 0-2 GHz in <10us. I am just wondering if we have that kind of device.
Your response is highly appreciated. Thank you.
Hey Donjie,
We do have several high-speed DACs that are capable of DDS, however they are not capable of programmable chirps and can only generate a single tone per SPI write. The DAC39RF10 does have a fast SPI link that can update the NCO fairly quickly, however this will require a fast-programming device like an FPGA to push all the necessary NCO words to the device in real time to generate the chirp.
So the question becomes what kind of resolution would they need between tones? How many tones would they need between 0 and 2GHz? From there we could extrapolate if it was possible to do if we have a high speed FPGA to program the device. This is quite a bit of overhead however.
Thanks and Regards,
Matt
This is noted Matthew. I appreciate the help and thank you for the response. Will relay this to the customer.