Part Number: DAC38RF82
Other Parts Discussed in Thread: TEST2
Hi team,
DAC38RF82 with mode LMFSHD=81180 is being used and the configuration is as below. The JESD204B LINK is ok, but there is no output when trying to give the data. The input clock is 562.5MHz, and the Sample Rate is 9 GSPS.
wr_da 0x00f863
wr_da 0x007863
wr_da 0x013080
rd_da 0xff10000
wr_da 0x007863
wr_da 0x090003
wr_da 0x2f0000
wr_da 0x300000
wr_da 0x0a0010
wr_da 0x0c2402
wr_da 0x0d0001
wr_da 0x190001
wr_da 0x090003
wr_da 0x253100
wr_da 0x272020
wr_da 0x280330
wr_da 0x280330
wr_da 0x090003
wr_da 0x4aff03
wr_da 0x5f0123
wr_da 0x604567
wr_da 0x090003
wr_da 0x4b1300
wr_da 0x4c1307
wr_da 0x4d0007
wr_da 0x4e0727
wr_da 0x4f1c60
wr_da 0x5100ff
wr_da 0x090004
wr_da 0x0b0004
wr_da 0x0c2502
wr_da 0x241001
wr_da 0x320708
wr_da 0x310b08
wr_da 0x310408
wr_da 0x33c730
wr_da 0x090000
rd_da 0x860000
wr_da 0x090004
wr_da 0x3b0000
wr_da 0x3c8029
wr_da 0x1b0100
wr_da 0x3e0909
wr_da 0x0df000
wr_da 0x090003
wr_da 0x240000
wr_da 0x5c0000
wr_da 0x090004
wr_da 0x0df000
wr_da 0x0ae802
wr_da 0x090004
wr_da 0x0a6802
wr_da 0x090000
wr_da 0x007863
wr_da 0x090003
wr_da 0x240020
wr_da 0x090003
wr_da 0x5c0003
wr_da 0x090000
wr_da 0x007862
wr_da 0x090000
wr_da 0x040000
wr_da 0x050000
wr_da 0x090003
wr_da 0x640000
wr_da 0x650000
wr_da 0x660000
wr_da 0x670000
wr_da 0x680000
wr_da 0x690000
wr_da 0x6a0000
wr_da 0x6b0000
wr_da 0x6c0000
wr_da 0x6d0000
wr_da 0x090003
rd_da 0xe40000
Could you help check is there anything need to be taken care of? Thanks.
Best Regards,
Cherry