Other Parts Discussed in Thread: CC1125, CC1200
Some of the sub 1 GHz RF transceiver devices like CC1200, CC1125, CC1311 etc specify that for additional band support (frequency bands 137 to 158 MHz) we need to contact TI. Kindly provide details of how to use these bands. Also provide details for if these devices can be used in continuous bands from 137 to 172 MHz.