Other Parts Discussed in Thread: AFE7686,
Hello,
we are trying to run the boundary scan test on our AFE7444 (using AFE7686 bsdl model).
The device JTAG port is chain connected with other IEE1149 compliant devices.
When the AFE7444 is tested individually (no JTAG chain), we can read the correct IDCODE, while when connected in chain, it seems that the chain is broken on AFE7444.
My first question is if the AFE7444 is IEEE1149.1 compliant
If yes, there are any specific settings or procedures that we should follow in order to run the test?
Thank you
Regards
Massimo