This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7900EVM: What is the supported temperature range ?

Part Number: AFE7900EVM

I would like to know the supported temperature range of the evaluation board AFE7900EVM ? Is there a version of this board that supports industrial temperature range (-40 to +85°C) ?

Thanks.

  • Hi Florian,

    Our EVM is designed to be operated at room temperature, 25°C. You certainly can try to operate the entire EVM within this temperature range, however TI cannot guarantee that it will work. The AFE itself is rated for this temperature range, but that won't be the issue. The issue would come from some accessory part(s)/IC(s)s on this EVM not being able to operate within this range. 

    Regards, Chase