Part Number: AFE7900EVM
I've followed TI204c-setup exactly. I'm producing a 1.83GHz signal, and getting the following result:
1.83GHz signal, 1800 NCO
This looks great and as expected.
Now, move the signal down to 1.5GHz:
1.5GHz signal, 1800 NCO
This has obviously gone awry. Something is happening at DC (although why it's flat isn't clear to me). Also several spurs.
If I move the signal down to 1.45GHz, the output is virtually indistinguishable:
1.45GHz signal, 1800 NCO
Same problem.
So, try again with the NCO at 1500:
1.55GHz signal, 1500 NCO
All sorts of problems here.
I'm guessing this has something to do with the ADC sample rate being around 3GS/s? Is this expected behavior? Is there a recommendation on how to sample in this frequency range?
Second question: Using latte, what are the steps to change the sample rate to something other than 737.28MS/s?
Thank you in advance!