Other Parts Discussed in Thread: AFE7920
Hi,
We are planning to use AFE7920EVM for our testing with Xilinx VCU118 board.
For configuring the device, we are planning to use USB to SPI interface, available on AFE7920 eval board with the help of AFE7920 eval GUI, rather than using SPI interface available on FMC connector.
I think TI has used TSW14J56EVM for testing.
That's why I want to know whether we can use Xilinx VCU118 board for testing.
Also, are there options available in GUI for configuring AFE7920 for custom cases other than some pre-defined example use cases in the GUI?
For example, I want to test AFE7920 with four SerDes lanes at 24.33024 gbps. Is it possible?
An early response is highly appreciated.
Thanks,
Lalit