Sorry for the repost, but I'm not sure using the "ask related question" option worked because I got no responses.
Using the AFE7950EVM with TSW14J57 generator/capture board:
I have a programmable supply on both the AFE7950EVM, set at 5.5V (and it doesn't droop; at the test point even when drawing about 3 amps, it stays at 5.5V) and 12V going into the TSW14J57 board.
running through the tutorial ppt slides, I'm not getting any errors, and PLL2 Locked stays lit, but the TSW board D2 led only flashes during programming, and keeps flashing after running the S1 script. However, it goes out when i hit the "send" button in the DAC screen of the HSDC Pro software. I get no output from TXA on the AFE board (or any of the TX), and the only connection I've made is from the SMA connector at TXA to a spectrum analyzer. My SA has a BW of 7.5GHz and I'm not seeing anything, no matter where I zoom in. The SA has an input impedance of 50 ohms and its noise floor is at about -80dBm.
I'm not getting any JESD errors and don't have to run the AFE.adcDacSync() command, though I've tried without and with running that.
D3 (PLL2 locked) is on. The tutorial doesn't talk about it, but D4 on the AFEEVM (LMK locked) never comes on. not sure what thats for, but I'm guessing it's maybe just for when an ext 10MHz sync clock is used.
As I said, on the TSW board, after running S1 but *before* hitting the Send button in HSDC Pro, D2 is blinking, D3 is on and steady, D5 and D6 are on but dim? (maybe meaning they're actually flashing at hf), D8 and D9 are on. The rest (D1, D4, D7) are off. On the AFE EVM board, *only* D3 (pll2 locked) is on.
As soon as I hit send (per the last post, I was told the tutorial was incorrect in stating that I should hit send before running the S1 script), on the TSW board, D1 (TX sync) flashes momentarily, and D2 turns off, and stays off. D3 remains on.
I get no signal on the TXA output. again, I have no other wires connected, on the coax from TXA to my spectrum analyzer.