Part Number: AFE8030EVM
Other Parts Discussed in Thread: AFE8030, LMK04828
Hi Team,
We have 6 EVMs and all of them have been modified for SPI access via FMC. Following changes have been made:
- The resistors connecting FMC pins to SPI signals have been mounted and the resistors connecting FTDI signals to SPI signals have been removed.
- Resistors connecting FMC pins to LMK SPI signals have been mounted and the resistors connecting FTDI signals to SPI signals have been removed.
- Resistors have been mounted to get JESD core clock from LMK to FMC.
Initially, on 4 of the EVMs, I couldn’t access the AFE chip via SPI. Then I connected the USB cable to the EVM and the FTDI part got powered up and things started working! I could do SPI access and read chip ID for example. So, now I have connected the 5V SOURCE to the 5V IN of the FTDI chip. I have disconnected the USB VBUS pin from feeding the FTDI chip. Is this a proper thing to do? The SPI and LMK_SPI signals are being driven from the FMC connector. Two of the EVMs work without this modification. and 4 EVMs which I am not able to access AFE chip but i am able to program the LMK can you please help with this .