This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7900EVM: Capture two Rx path in the same time

Part Number: AFE7900EVM
Other Parts Discussed in Thread: AFE7900

Hi, 

I am evaluating AFE7900 with TSW14J58. Is it possible to capture synchronously two Rx path  ? 

Fayçal

  • Hi Haizouni,

    At this moment we do not have the capability to capture two Rx channels synchronously with the TSW14J58. I have informed our SW team about this issue and will request that this feature be added in the next design. 

    If synchronous capture of two Rx channels is required then one path that can be done is to use our TI204c-IP and create a design for the AFE+TSW14J58, so that you can capture the data through Vivado. To receive access to the TI204c-IP you can request permission through the link below.

    https://www.ti.com/tool/TI-JESD204-IP 

    Regards,

    David Chaparro