Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950,
Hello, team
Can I use the AFE7950 alone without the FPGA board?
I connected the EVM board with usb interface under latte,after bring up, and run mode5,the current of the EVM is about 1.1A, but the loopback function dosenot work, the DAC output noting.
I tested RXA-TXA and RXB-TXB, none of them work.
so I want to know can the EVM board work in loopback mode without FPGA board.