Part Number: TRF1208-AFE7950EVM
Other Parts Discussed in Thread: TSW14J57EVM, AFE7950
Hi Team
We are trying to interface TRF1208-AFE7950EVM with TSW14J57EVM and followed a bring-up presentation to interface both these devices to test the basic signal generation and capture capabilities of AFE7950. However, we are running into errors even after several retries. The error screenshot on the latte is as follows:

The process we have followed is mentioned in the presentation by the name: "AFE7950+TSW14J57" available in "AFE79xxEVM_TSW14J57_BringupGuides" folder in the secure folder.
Can you please help us resolve this error and share the reason for this error?
The log is as follows:
#Executing .. AFE7950/bringup/setup.py
#Start Time 2023-11-27 11:38:18.747000
AFE79xxLibraryPG1p0
spi - USB Instrument created.
resetDevice
Purge
Kintex RegProgrammer - USB Instrument created.
Kintex RegProgrammer - USB Instrument created.
Kintex RegProgrammer - USB Instrument created.
#Done executing .. AFE7950/bringup/setup.py
#End Time 2023-11-27 11:38:25.627000
#Execution Time = 6.88000011444 s
#================ ERRORS:0, WARNINGS:0 ================#
#======
#Executing .. AFE7950/bringup/devInit.py
#Start Time 2023-11-27 11:39:13.658000
Power Card - USB Instrument created.
Reset the FPGA and try again.
Device with name CPLD already exist. Please change the name to get new device.
Loaded Libraries
Refreshed GUI
#Done executing .. AFE7950/bringup/devInit.py
#End Time 2023-11-27 11:39:19.540000
#Execution Time = 5.88199996948 s
#================ ERRORS:1, WARNINGS:1 ================#
#======
#Executing .. AFE7950/bringup/S1_OnboardClk_RX_250M_TX_FB_500M.py
#Start Time 2023-11-27 11:43:38.822000
The External Sysref Frequency should be an integer factor of: 3.84MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
LMK Clock Divider - Device registers reset.
LMK Clock Divider - Device registers reset.
REFCLOCK is used from LMK source, ensure board connections are ok to do the same
LMK and FPGA Configured.
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x11
AFE Reset Done
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
//Firmware Version = 11000
//PG Version = 1
//Release Date [dd/mm/yy] = 10/7/19
patchSize=11697
//Patch Version = 165
//PG Version = 0
//Release Date [dd/mm/yy] = 27/11/21
AFE MCU Wake up done and patch loaded.
PLL Locked
AFE PLL Configured.
AFE SerDes Configured.
AFE Digital Chains configured.
AFE TX Analog configured.
AFE RX Analog configured.
AFE FB Analog configured.
AFE JESD configured.
AFE AGC configured.
AFE GPIO configured.
Sysref Read as expected
###########Device DAC JESD-RX 0 Link Status###########
Serdes-FIFO error for lane 0: 1
Serdes-FIFO error for lane 1: 1
Serdes-FIFO error for lane 2: 1
Serdes-FIFO error for lane 3: 1
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 0; Alarms: 0xf000
###################################
###########Device DAC JESD-RX 1 Link Status###########
Serdes-FIFO error for lane 0: 1
Serdes-FIFO error for lane 1: 1
Serdes-FIFO error for lane 2: 1
Serdes-FIFO error for lane 3: 1
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 1; Alarms: 0xf000
###################################
AFE Configuration Complete
#Done executing .. AFE7950/bringup/S1_OnboardClk_RX_250M_TX_FB_500M.py
#End Time 2023-11-27 11:44:12.372000
#Execution Time = 33.5499999523 s
#================ ERRORS:18, WARNINGS:1 ================#
SPIA has Not got control of PLL pages
###########Device DAC JESD-RX 0 Link Status###########
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 0; Alarms: 0x0
###################################
###########Device DAC JESD-RX 1 Link Status###########
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 1; Alarms: 0x0
###################################
#======
SPIA has Not got control of PLL pages
###########Device DAC JESD-RX 0 Link Status###########
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 0; Alarms: 0x0
###################################
###########Device DAC JESD-RX 1 Link Status###########
Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane2: False; Please check if the transmitter is sending data and eye is good.
Comma Align Lock Lane3: False; Please check if the transmitter is sending data and eye is good.
CS State TX0: 0b00000000 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 1; Alarms: 0x0
###################################
#======
has context menu
Thanks and Regards
Vinit Bansal
+91-9632438652