This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7903: Buggy sysParams.txDataMux

Part Number: AFE7903

We are using the AFE7903 and try to get it running. In Latte we use 

sysParams.rxDataMux = [0,1,4,5,2,3,6,7] 

to map RX1 and and RX3 to JESD lane STx1. This can be seen on the following picture

On the other side we have to use TX2 and TX4. 

If we use the logical setting

sysParams.txDataMux = [2,3,6,7,0,1,4,5]

we are unable to generate data. Data from the FPGA gets not sent out. Also working with sysParams.jesdLoopbackEn dont work. If we change the data mux to 

sysParams.txDataMux = [6,7,2,3,4,5,0,1]

everything works fine besides that he channels arriving are mixed up at the FPGA. Maybe it has to do with my other problems described here https://e2e.ti.com/support/rf-microwave-group/rf-microwave/f/rf-microwave-forum/1305315/afe7903-confusing-data-mux

The txDataMux seems to be buggy. Can you confirm this? Or how to use it the correct way? 

  • Hi Christian,

    I have tried this and I do not see an output out of the DAC when using the sysParams.txDataMux = [2,3,6,7,0,1,4,5] setting and having only TXB and TXD enabled.

    I will reach out to the software team so that they can advise.

    In the meantime, could you please post your configuration to make sure everything else is correct and so that we can test the same use case?

    Best,

    Camilo

  • Hi Camilo

    I will send you the configuration in a private message. It contains to much project specific comments to post it in public.

  • Hi Christian, 

    Thank you, we will make sure to review and get back to you with the advise from the software team.

    Best,

    Camilo

  • Hi Christian, 

    Thank you for the patience. The correct setting should be sysParams.txDataMux = [6,7,0,1,4,5,2,3]. I have tried this and was able to see the correct output out of both TX channels.

    Best,

    Camilo

  • Hi Christian,

    I've unlocked this thread so that we can continue discussion on this topic. I understand you and Camilo have had some further discussion - would you mind please describing what the current issue is and what we can do to help? 

    Thanks!

    Aman

  • Hi Aman

    For me it seems that the configureDacDataMux() of the mJesdSubchip.py is buggy. I played with the registers and have now some correct values. Maybe not everything is correct, but I get the correct loopback routing. I'm now using the logic DataMux settings and added some raw register settings. 

    sysParams.rxDataMux		= [0,1,4,5,2,3,6,7]
    sysParams.txDataMux		= [2,3,6,7,0,1,4,5]
    
    #Fix wrong muxes set by sysParams.txDataMux
    #Gain access to JESD_SUBCHIP
    AFE.regs.writeReg(0x0016,0x10)
    #fix TXB
    AFE.regs.writeReg(0x00ce,0x00)
    AFE.regs.writeReg(0x0060,0x00)
    #fix TXD
    AFE.regs.writeReg(0x00d2,0x22)
    AFE.regs.writeReg(0x0061,0x11)
    #Release access to JESD_SUBCHIP
    AFE.regs.writeReg(0x0016,0x10)

    At the moment I use these settings and it works. But maybe I'm missing some registers.

  • Hi Christian,

    Thanks for updating me on this. Would you mind please clarifying which lanes you want to appear together in the link? I see in the top post that you would like RX 1 and 3 on the same lane for STX and TX 2 and 4 on the same lane for SRX.

    I also see that Camilo had provided this: sysParams.txDataMux = [6,7,0,1,4,5,2,3] - did this solution still give mixed-up signals at the FPGA?

    Thanks!

    Aman

  • Hi Aman

    As we use the the AFE7903 we only have two channels. We would like to use both with just one lane. RX1 -> TX2 and RX3 -> TX4

    Every solution either leads to mixed up channels or a unused but necessary second lane which we don't have.

    And yes, the sysParams.txDataMux = [6,7,0,1,4,5,2,3]  together with sysParams.rxDataMux = [0,1,4,5,2,3,6,7] gives a mixed-up signals. That's how it should be with this setting (0,1 to 6,7 / RX1 to TX4)

    Regards

    Christian

  • Hi Christian,

    Understood, thanks for the info. As I said, I'm working through these issues in order of priority, so I appreciate your patience on this issue. I will be sure to update you once I get have something to share.

    Thanks,

    Aman