This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7900EVM: Latter Error Message

Expert 1780 points

Part Number: AFE7900EVM

Hello,

     We have modified your reference design for ZCU102 to work for another ZU+ board. After programming from Latte, we got the following error message:

#Executing .. AFE79xx/bringup/TI_IP_10Gbps_8Lane_ConfigLmk.py
#Start Time 2023-12-26 17:54:57.291000 
The External Sysref Frequency should be an integer factor of: 3.84MHz
2T2R1F Number: 0
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
2T2R1F Number: 1
Valid Configuration: True
laneRateRx: 9830.4
laneRateFb: 9830.4
laneRateTx: 9830.4
Device Initialization for ChipVersion: 2.0
LMK Clock Divider - Device registers reset.
LMK Clock Divider - Device registers reset.
REFCLOCK is used from LMK source, ensure board connections are ok to do the same
DONOT_OPEN_Atharv_FULL - Device registers reset.
chipType: 0xa
chipId: 0x78
chipVersion: 0x20
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Fuse farm load autoload done successful
No autload error
Fuse farm load autoload done successful
No autload error
patchSize=6677
//Patch Version = 155
//PG Version = 0
//Release Date [dd/mm/yy] = 27/11/21
SPIA has got control of PLL pages
PLL Locked
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
SPIA has got control of PLL pages
PLL Pages SPI control relinquished.
Sysref Read as expected
###########Device DAC JESD-RX 0 Link Status###########
CS State TX0: 0b10101010 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 0; Alarms: 0x0
###################################
###########Device DAC JESD-RX 1 Link Status###########
CS State TX0: 0b10101010 . It is expected to be 0b10101010
FS State TX0: 0b00000000 . It is expected to be 0b01010101
Couldn't get the link up for device RX: 1; Alarms: 0x0
###################################
#Done executing .. AFE79xx/bringup/TI_IP_10Gbps_8Lane_ConfigLmk.py
#End Time 2023-12-26 17:56:13.144000
#Execution Time = 75.853000164 s 
#================ ERRORS:2, WARNINGS:1 ================#

CS State for JESD-RX 0 link is correct but FS state is not and the same is for Rx 1 link. 

Also, it speaks about the DAC JESD Link (i.e., JESD receive on the AFE); does it mean that the ADC link is working? 

Please help us debug the problem.

Thank you  in advance,