Part Number: AFE7769DEVM
Other Parts Discussed in Thread: TSW14J58EVM, AFE7769D
Currently I am struggling on the set up.
Here I have several questions.
Could the Latte software control the FPGA board(TSW14J58EVM) also?
When I open the Latte and HSDC together, USB connection lost.
It looks like the Latte could control the FPGA board but somehow FPGA is not correctly set up if I use Latte only.
Does the JTAG and Vivado are essential?
I thought JTAG is optional, and I did not use the JTAG connection. Could it be related with the FPGA set up issue of Latte?
I want to start testing TX first.
I am checking the TX port with SA and change settings.
I only could see the LO leakage for short period of time, and it disappeared.
So it means, AFE7769D could be set correctly, I guess there is no Baseband signal and it stopped.
Document sbasag4a page 174 shows the device can work with Fref down to 122.88Mhz.
I thought the AFE7769D could accept 122.88Mhz as a ref CLK but the Latte software config tab does not allow me to set.
The pull-down menu of config tab only shows 245.76MHz, 368.64MHz, 491.52Mhz
I think the config tab should includes the 122.88MHz on the pull-down menu.
When I start HSDC, I saw "Firmware version and dll version does not match" message.
How could I solve the issue?
Thank you in advance for the help.