Other Parts Discussed in Thread: LMX2572LP
Hello,
I am working with your AFE7071. As has been recommended elsewhere on this forum, I am using the LMX2572LP as the LO input to the AFE7071. I have two boards that I am attempting to calibrate. I am using the procedure documented in SLWU029D.
The first board achieves sideband suppression just fine with the phase and gain adjustments. With the first board, I can easily get the sideband suppression down into the -70dBm noise floor of the spectrum analyzer that is being used, with most any input power, 0 dBm to +3 dBm or more.
On the second board, with 3.8dBm in on the LO, by adjusting the gain and phase, I can only get the sideband about 40dB below the modulated output. If I reduce the LO input power to 0dBm, I can easily get the sideband suppression into the -70dBm noise floor. If I go up in frequency a little bit, I can fully suppress the sideband to the -70dB noise floor as well.
There is just one particular combination of frequency and input power on one particular board that is prevents the sideband from being supressed, and I am confused as to what might cause this.
Thank you