Other Parts Discussed in Thread: TSW14J58EVM, AFE8000
Hi TI,
I am currently running though the bring up process as provided with the AFE8000 connected to the TSW14J58EVM.
The Input ref signal to the LMK on the AFE8000 is correct to the bringup process.
I am trying to go through the software "bring up" but I keep getting the error below in the log file and the error below*2 in the terminal.
Log file error:
"Resetting FPGA Pin.
Reset the FPGA and try again."
Terminal output error:
"ERROR Please check environment setup! No device is detected."
I have included the log file and the terminal output for completeness.
I have a feeling it may be to do with the referenced FTDI Not Connected but all 3 USBs are connected to SS connections.
AFE80xxCatLibrary spi - USB Instrument created. resetDevice Kintex RegProgrammer - USB Instrument created. Kintex RegProgrammer - USB Instrument created. Kintex RegProgrammer - USB Instrument created. FPGA reset - USB Instrument created. Power Card - USB Instrument created. Version : 0x101204c Connected to Capture Card Loaded Libraries Loaded Configuration: AFE8000_SampleConfig.xlsx Refreshed the GUI. #================ ERRORS:0, WARNINGS:0 ================# Loaded Configuration: AFE8000_SampleConfig.xlsx Refreshed the GUI. Device Initialization for ChipVersion: 2.0 The External Sysref Frequency should be an integer factor of: 3.90625MHz 2T2R1F Number: 0 Valid Configuration: True laneRateRx: 24750.0 laneRateRx1: 24750.0 laneRateFb: 24750.0 laneRateTx0: 24750.0 laneRateTx1: 24750.0 2T2R1F Number: 1 Valid Configuration: True laneRateRx: 24750.0 laneRateRx1: 24750.0 laneRateFb: 24750.0 laneRateTx0: 24750.0 laneRateTx1: 24750.0 LMK Clock Divider - Device registers reset. LMK Clock Divider - Device registers reset. REFCLOCK is used from LMK source, ensure board connections are ok to do the same LMK and FPGA Configured. DONOT_OPEN_Afe80xx_FULL - Device registers reset. chipType: 0xa chipId: 0x8001 chipVersion: 0x20 Programing FPGA .... Resetting FPGA Pin. Reset the FPGA and try again. LMK and FPGA Configured. AFE Reset Done Fuse farm load autoload done successful No autload error Fuse farm load autoload done successful No autload error //Firmware Version = 9108 //PG Version = 1 //Release Date [dd/mm/yy] = 28/8/20 //Patch Version = 0 //PG Version = 0 //Release Date [dd/mm/yy] = 0/0/0 AFE MCU Wake up done and patch loaded. PLL Locked AFE PLL Configured. AFE SerDes Configured. AFE Digital Chains configured. AFE TX Analog configured. AFE RX Analog configured. AFE FB Analog configured. AFE JESD configured. AFE AGC configured. AFE PAP and Alarms configured. AFE GPIO configured. Sysref Read as expected Setting RBD to: 11 Setting RBD to: 11 Programing FPGA .... Resetting FPGA Pin. Version : 0x101204c Connected to Capture Card FPGA Tx sysref captured FPGA Rx sysref captured Setting RBD to: 11 ###########Device DAC JESD-RX 0 Link Status########### CS State TX0: 0b00000000 . It is expected to be 0b10101010 BUF State TX0: 0b00000000 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 0 ################################### ###########Device DAC JESD-RX 1 Link Status########### CS State TX0: 0b10101010 . It is expected to be 0b10101010 BUF State TX0: 0b00000000 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 1 ################################### AFE Configuration Complete #================ ERRORS:3, WARNINGS:0 ================# Loaded Configuration: AFE8000_SampleConfig.xlsx Refreshed the GUI. Device Initialization for ChipVersion: 2.0 The External Sysref Frequency should be an integer factor of: 3.90625MHz 2T2R1F Number: 0 Valid Configuration: True laneRateRx: 24750.0 laneRateRx1: 24750.0 laneRateFb: 24750.0 laneRateTx0: 24750.0 laneRateTx1: 24750.0 2T2R1F Number: 1 Valid Configuration: True laneRateRx: 24750.0 laneRateRx1: 24750.0 laneRateFb: 24750.0 laneRateTx0: 24750.0 laneRateTx1: 24750.0 LMK Clock Divider - Device registers reset. LMK Clock Divider - Device registers reset. REFCLOCK is used from LMK source, ensure board connections are ok to do the same LMK and FPGA Configured. DONOT_OPEN_Afe80xx_FULL - Device registers reset. chipType: 0xa chipId: 0x8001 chipVersion: 0x20 Programing FPGA .... Resetting FPGA Pin. Reset the FPGA and try again. LMK and FPGA Configured. AFE Reset Done Fuse farm load autoload done successful No autload error Fuse farm load autoload done successful No autload error //Firmware Version = 9108 //PG Version = 1 //Release Date [dd/mm/yy] = 28/8/20 //Patch Version = 0 //PG Version = 0 //Release Date [dd/mm/yy] = 0/0/0 AFE MCU Wake up done and patch loaded. PLL Locked AFE PLL Configured. AFE SerDes Configured. AFE Digital Chains configured. AFE TX Analog configured. AFE RX Analog configured. AFE FB Analog configured. AFE JESD configured. AFE AGC configured. AFE PAP and Alarms configured. AFE GPIO configured. Sysref Read as expected Setting RBD to: 11 Setting RBD to: 11 Programing FPGA .... Resetting FPGA Pin. Version : 0x101204c Connected to Capture Card FPGA Tx sysref captured FPGA Rx sysref captured Setting RBD to: 11 ###########Device DAC JESD-RX 0 Link Status########### CS State TX0: 0b00000000 . It is expected to be 0b10101010 BUF State TX0: 0b00000000 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 0 ################################### ###########Device DAC JESD-RX 1 Link Status########### CS State TX0: 0b10101010 . It is expected to be 0b10101010 BUF State TX0: 0b00000000 . It is expected to be 0b11111111 Couldn't get the link up for device RX: 1 ################################### AFE Configuration Complete #================ ERRORS:3, WARNINGS:0 ================#
Connecting... 1 Detected 1 device(s) connected. DEVICE[0] Flags = 4 Type = 0 ID = 0X0403601F LocId = 0 SerialNumber = FT83SUUQ Description = TSW14J58 Creating ftd3xx.ftd3xx.FTD3XX object at 0x000002441E3D7F28 Library Version 0X1030002 Driver Version 0X1030008 Firmware Version 0X000109 USB 784 True Chip Configuration VendorID = 0x0403 ProductID = 0x601f StringDescriptors Manufacturer = FTDI ProductDescription = TSW14J58 SerialNumber = FT83SUUQ InterruptInterval = 0x09 PowerAttributes = 0xa0 (Bus-powered Remote wakeup) PowerConsumption = 0x60 Reserved2 = 0x00 FIFOClock = 0x00 (100 MHz) FIFOMode = 0x01 (600 Mode) ChannelConfig = 0x02 (1 Channel) OptionalFeatureSupport = 0x0000 BatteryChargingEnabled 0 DisableCancelOnUnderrun 0 NotificationEnabled 0 0 0 0 UnderrunEnabled 0 0 0 0 EnableFifoInSuspend 0 DisableChipPowerdown 0 BatteryChargingGPIOConfig = 0x0 FlashEEPROMDetection = 0x10 (read-only) Custom Config Validity Valid Custom Config Checksum Valid GPIO Input Ignore Config Used Custom MSIO_Control = 0x00010800 GPIO_Control = 0x00000000 Connected Opened the USB FTDI Handle. Closing the USB FTDI Handle. Instantiated Class lmkLib Instantiated Class fpgaLib_J58 Instantiated Class RRFLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class FbDigLib Instantiated Class AGCLib Instantiated Class FbDDCLib Instantiated Class FbDGCLib Instantiated Class FbDSAGPEC Instantiated Class FbDCCorrLib Instantiated Class FbPrgmDlyLib Instantiated Class FbNLCLib Instantiated Class FbDCEstimLib Instantiated Class RxFbDsaLib Instantiated Class TTLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class RRFLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class RxDigLib Instantiated Class AGCLib Instantiated Class RxDDCLib Instantiated Class RxDSAGPEC Instantiated Class ALCLib Instantiated Class RxNLCLib Instantiated Class RxDCCorrLib Instantiated Class RxDGCLib Instantiated Class RxPrgmDlyLib Instantiated Class RxFbDsaLib Instantiated Class FbDigLib Instantiated Class AGCLib Instantiated Class FbDDCLib Instantiated Class FbDGCLib Instantiated Class FbDSAGPEC Instantiated Class FbDCCorrLib Instantiated Class FbPrgmDlyLib Instantiated Class FbNLCLib Instantiated Class FbDCEstimLib Instantiated Class RxFbDsaLib Instantiated Class TTLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TxDigLib Instantiated Class TxILIQCorrLib Instantiated Class TopLib Instantiated Class pllLib Instantiated Class TimingController Instantiated Class IoWrapLib Instantiated Class JESDLib Instantiated Class DACJesdLib Instantiated Class DACJesdLib Instantiated Class ADCJesdLib Instantiated Class ADCJesdLib Instantiated Class serdesLib Instantiated Class serdesLib Instantiated Class jesdSubchipLib Instantiated Class DsaLib Instantiated Class TopProcLib Instantiated Class CalibTopHw Instantiated Class MacroLib Instantiated Class MacroHWLib Instantiated Class MacroErrLib Instantiated Class MacroHWLib Instantiated Class DProc1Lib Instantiated Class DProc1FwProgLib Instantiated Class DProc1FwDbgLib Instantiated Class DProc1MailboxLib Opened the USB FTDI Handle. Closing the USB FTDI Handle. Instantiated Class cpldLib couldn't create image from httpscdn4.iconfinder.comdataiconsionicons512icon-plus-round-128.png libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream Opened the USB FTDI Handle. Closing the USB FTDI Handle. libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream libpng warning zTXt Data error in compressed datastream Opened the USB FTDI Handle. Closing the USB FTDI Handle. Opened the USB FTDI Handle. Closing the USB FTDI Handle. Deleting Handle.. Connecting... 0 ERROR Please check environment setup! No device is detected. FTDI Not Connected FPGA not connected. Function reset skipped. FPGA not connected. Function checkVersion skipped. FPGA not connected. Function fpgaTxConfig skipped. FPGA not connected. Function selectDrive skipped. FPGA not connected. Function fpgaRxConfig skipped. FPGA not connected. Function selectCapture skipped. FPGA not connected. Function fpgaJesdReset skipped. FPGA not connected. Function fpgaSysref skipped. FPGA not connected. Function fpgaSysrefCheck skipped. FPGA not connected. Function fpgaJesdReset skipped. FPGA not connected. Function fpgaSysref skipped. FPGA not connected. Function fpgaSysrefCheck skipped. FPGA not connected. Function fpgaJesdReset skipped. FPGA not connected. Function fpgaSysref skipped. FPGA not connected. Function fpgaSysrefCheck skipped. Deleting Handle.. Connecting... 1 Detected 1 device(s) connected. DEVICE[0] Flags = 4 Type = 0 ID = 0X0403601F LocId = 0 SerialNumber = FT83SUUQ Description = TSW14J58 Creating ftd3xx.ftd3xx.FTD3XX object at 0x000002442FFF5F60 Library Version 0X1030002 Driver Version 0X1030008 Firmware Version 0X000109 USB 784 True Chip Configuration VendorID = 0x0403 ProductID = 0x601f StringDescriptors Manufacturer = FTDI ProductDescription = TSW14J58 SerialNumber = FT83SUUQ InterruptInterval = 0x09 PowerAttributes = 0xa0 (Bus-powered Remote wakeup) PowerConsumption = 0x60 Reserved2 = 0x00 FIFOClock = 0x00 (100 MHz) FIFOMode = 0x01 (600 Mode) ChannelConfig = 0x02 (1 Channel) OptionalFeatureSupport = 0x0000 BatteryChargingEnabled 0 DisableCancelOnUnderrun 0 NotificationEnabled 0 0 0 0 UnderrunEnabled 0 0 0 0 EnableFifoInSuspend 0 DisableChipPowerdown 0 BatteryChargingGPIOConfig = 0x0 FlashEEPROMDetection = 0x10 (read-only) Custom Config Validity Valid Custom Config Checksum Valid GPIO Input Ignore Config Used Custom MSIO_Control = 0x00010800 GPIO_Control = 0x00000000 Connected (32, 396000.0) (1, 12375.0) PLL Rate Configured 12375.0 ('DRP Read ', '00000018') 0001310C 00000008 ('DRP Write ', '00000018 00000008') ('DRP Read ', '00000018') 0001310C 00000020 ('DRP Write ', '00000018 00000020') 99.0 Selected OUTDIV 1 Selected HalfRate 1 Selected N 99 0001300C 00000008 ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') 00013008 00000002 ('DRP Write ', '0000000E 00000001') ('DRP Write ', '0000000E 00000001') 00016008 00000002 ('DRP Write ', '0000000E 00000001') ('DRP Write ', '0000000E 00000001') Common 00013008 00000002 Select interface ('DRP Read ', '0000000E') 0001310C 00000001 ('HALFRATE ', 1) ('DRP Read ', '00000014') 0001310C 00000061 ('FBDIV', 97) ('DRP Write ', '00000014 00000061') ('DRP Write ', '00000014 00000061') 00016008 00000002 ('DRP Read ', '0000000E') 0001610C 00000001 ('HALFRATE ', 1) ('DRP Read ', '00000014') 0001610C 00000061 ('FBDIV', 97) ('DRP Write ', '00000014 00000061') ('DRP Write ', '00000014 00000061') ('TX Lanes ', [5]) TX_SW0 00000000 TX_SW1 00000000 StreamConfig 00060033 Stream 0 24.0115.2 Gbps 20.83% Stream 1 0115.2 Gbps 0.00% 00010004 00020000 00011020 00000000 00012020 00000000 00011060 00000002 00012060 00000032 Opened the USB FTDI Handle. Closing the USB FTDI Handle. Opened the USB FTDI Handle. Closing the USB FTDI Handle. Deleting Handle.. Connecting... 0 ERROR Please check environment setup! No device is detected. FTDI Not Connected FPGA not connected. Function reset skipped. FPGA not connected. Function checkVersion skipped. FPGA not connected. Function fpgaTxConfig skipped. FPGA not connected. Function selectDrive skipped. FPGA not connected. Function fpgaRxConfig skipped. FPGA not connected. Function selectCapture skipped. FPGA not connected. Function fpgaJesdReset skipped. FPGA not connected. Function fpgaSysref skipped. FPGA not connected. Function fpgaSysrefCheck skipped. FPGA not connected. Function fpgaJesdReset skipped. FPGA not connected. Function fpgaSysref skipped. FPGA not connected. Function fpgaSysrefCheck skipped. FPGA not connected. Function fpgaJesdReset skipped. FPGA not connected. Function fpgaSysref skipped. FPGA not connected. Function fpgaSysrefCheck skipped. Deleting Handle.. Connecting... 1 Detected 1 device(s) connected. DEVICE[0] Flags = 4 Type = 0 ID = 0X0403601F LocId = 0 SerialNumber = FT83SUUQ Description = TSW14J58 Creating ftd3xx.ftd3xx.FTD3XX object at 0x000002442D8A4F28 Library Version 0X1030002 Driver Version 0X1030008 Firmware Version 0X000109 USB 784 True Chip Configuration VendorID = 0x0403 ProductID = 0x601f StringDescriptors Manufacturer = FTDI ProductDescription = TSW14J58 SerialNumber = FT83SUUQ InterruptInterval = 0x09 PowerAttributes = 0xa0 (Bus-powered Remote wakeup) PowerConsumption = 0x60 Reserved2 = 0x00 FIFOClock = 0x00 (100 MHz) FIFOMode = 0x01 (600 Mode) ChannelConfig = 0x02 (1 Channel) OptionalFeatureSupport = 0x0000 BatteryChargingEnabled 0 DisableCancelOnUnderrun 0 NotificationEnabled 0 0 0 0 UnderrunEnabled 0 0 0 0 EnableFifoInSuspend 0 DisableChipPowerdown 0 BatteryChargingGPIOConfig = 0x0 FlashEEPROMDetection = 0x10 (read-only) Custom Config Validity Valid Custom Config Checksum Valid GPIO Input Ignore Config Used Custom MSIO_Control = 0x00010800 GPIO_Control = 0x00000000 Connected (32, 396000.0) (1, 12375.0) PLL Rate Configured 12375.0 ('DRP Read ', '00000018') 0001310C 00000008 ('DRP Write ', '00000018 00000008') ('DRP Read ', '00000018') 0001310C 00000020 ('DRP Write ', '00000018 00000020') 99.0 Selected OUTDIV 1 Selected HalfRate 1 Selected N 99 0001300C 00000008 ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001320C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001320C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001320C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001320C 000000C0 ('DRP Write ', '00000063 000000C0') ('DRP Read ', '0000007C') 0001620C 00002068 ('TXOUT', '0x2068') ('DRP Read ', '00000063') 0001620C 000000C0 ('RXOUT', '0xc0') ('DRP Read ', '0000007C') 0001620C 00002068 ('DRP Write ', '0000007C 00002068') ('DRP Read ', '00000063') 0001620C 000000C0 ('DRP Write ', '00000063 000000C0') 00013008 00000002 ('DRP Write ', '0000000E 00000001') ('DRP Write ', '0000000E 00000001') 00016008 00000002 ('DRP Write ', '0000000E 00000001') ('DRP Write ', '0000000E 00000001') Common 00013008 00000002 Select interface ('DRP Read ', '0000000E') 0001310C 00000001 ('HALFRATE ', 1) ('DRP Read ', '00000014') 0001310C 00000061 ('FBDIV', 97) ('DRP Write ', '00000014 00000061') ('DRP Write ', '00000014 00000061') 00016008 00000002 ('DRP Read ', '0000000E') 0001610C 00000001 ('HALFRATE ', 1) ('DRP Read ', '00000014') 0001610C 00000061 ('FBDIV', 97) ('DRP Write ', '00000014 00000061') ('DRP Write ', '00000014 00000061') ('TX Lanes ', [5]) TX_SW0 00000000 TX_SW1 00000000 StreamConfig 00060033 Stream 0 24.0115.2 Gbps 20.83% Stream 1 0115.2 Gbps 0.00% 00010004 00020000 00011020 00000000 00012020 00000000 00011060 00000002 00012060 00000032
I have had these boards working in the past but they have all of a sudden become extremely difficult to get working.
Any help would be greatly appreciated.
Kind regards
Oliver Forbes-Shaw