This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: SPUR mirrored around REF_CLK_HIGH/2

Part Number: AFE7950EVM
Other Parts Discussed in Thread: TSW14J58EVM

Using the TSW14J58EVM  DC182_A7 to connect to the AFE7950EVM DC135 REV A

Default bringup scripts for external clocks with both 204B and 204C from TI-AFE79xx-Latte_V2p4p1.exe

I'm seeing a TX SPUR mirrored about the REF_CLK_HIGH/2 frequency. So for 204C I'm getting the results in the table below. Clock source phase noise is less than -55 dBc/Hz 3Hz away.

Are you aware of any settings I can fiddle with to try and remove these SPURS?

Fund (GHz dBm)  SPUR (GHz dBm)
1.5 -12                 10.3 -21
2.5 -11                 9.3 -18
3.5 -5                   8.3 -14
4.5 -1.5                7.3 -9
5.5 -2.4                6.3 -6
6.5 -5                   5.3 -4
7.5 -6                   4.3 -5
8.5 -7                   3.3 -15
9.5 -7                   2.3 -24

Thanks, David.