Part Number: DAC38RF93
hello all,
In our design we use with high speed DAC38RF93.
In one of our application we need to work with sampling rate of 7920MHz (using the internal PLL).
The internal PLL have two VCO's with ranges: 1: VCO0 - 5240MHz to 6720MHz, 2: VCO1 – 7960MHz to 9000MHz.
Because we work outside the range of VCO1 we want to know what the KVCO of VCO1 (Fout VS Vtune graph) for stability analysis.
I want to mention that I tried this configuration at room temperature and it work ok, but we need to proof that the system is stable in this mode.
Can I get this parameter? And maybe someone can add some extra data about the stability of the PLL/VCO in this frequency.
thanks ahead,
Peleg bs