This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950: SERDES IBIS Model loading error

Part Number: AFE7950

Dear All,

We're facing error in loading IBIS model in Zuken Cadstar 

(line   74) - Parameter file hummingbird_rx.ami not found.
(line   75) - Code file hummingbird_rx_64.dll not found.
(line  251) - Code file hummingbird_tx_64.so not found.
(line  251) - Parameter file hummingbird_tx.ami not found.
(line  252) - Code file hummingbird_tx_64.dll not found.
 
Import of device 'AFE79XABJ' from vendor 'TI'
- Equally named model 'obuf_10_typ_in' is defined in IBIS file 'C:\Users\dbpat\Documents\DESIGNER INFORMATION\AFE79xx_IBIS_models\afe79xx_cmos.ibs'.
Please help us to resolve the issue.
Thanks in advance.
Regards,
Abhishek
  • Hi Abhishek,

    After reviewing the files we found that there was a naming issue which has now been fixed. Please download the IBIS Model that is now available in the secure folder and you should no longer receive this error.

    Regards,

    David Chaparro 

  • Dear David, 

    Now there are few new error came.

    Please can you fix and check if it works fine?

    Thanks in advance.

    Regards,

    Abhishek

  • Hi Abhishek,


    I have verified the new files using the HyperLynx tool and I do not see these errors, so it looks like these may be specific to the tool you are using. 

    Based on the errors you are seeing the Rx_Dj, Rx_Rj, and Rx_Noise parameters should be moved to the 'Reserved Parameters' section of the AMI file. 

    I have made these changes and will be sending you an updated Rx AMI file with these changes through the E2E chat that we have open. 

    Also, are you using a Windows or Linux OS for these simulations? 

    Regards,

    David Chaparro