Other Parts Discussed in Thread: SYSCONFIG
Hi team,
I am using the rfWakeOnRadioTx example for LP1352P2. Originally it is designed to work at Sub-1 GHz. I would like to use it at 2.4 GHz, so I am trying to change the frequency on SysConfig, but I can't select high PA. When I try to do it, it shows the following warning:
Then if I go to Device Configuration an disable the Force VDDR option, it doesn't let me select a TX Power value higher than 5 dBm. Even if I ignore this warning, the highest value of TX Power it allows me to set is 14 dBm.
How do I enable the 20 dBm (high PA) in this case?
Thank you in advance,
Eduardo.