Other Parts Discussed in Thread: AFE7900
Is there any mismatch between the Xilinx KC705 and AFE7900 regarding to TI-JESD IP and FMC voltage levels?
As far as I know the default voltage level for FMC banks are 2.5V, but can be changed to 1.8V.
AFE7900 is working with 1.8V. Do I have to modify the KC705 FMC voltage to 1.8V or 2.5v can work with AFE7900 without problem?
Is there any reference design regarding to KC705 with AFE7900?
Thanks in advance,
Berk