This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: Simultaneous Tx Rx with TSW14J58EVM and AFE7950

Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950, TSW14J58EVM

Tool/software:

I am using TSW14J58EVM with AFE7950 and would like to record 2Rx channels while transmitting 1Tx channel.
It seems that synchronized operation isn't possible so until it is I would like to use a less demanding setup :


1. The Rx and Tx needn't be synchronized (nevertheless, they should overlap most of the time).
2. SW init ("trigger") - no need for external HW trigger.
3. Tx and Rx would be memory based (I generate the Tx signal and analyze the Rx signals in python).

4. Max Bandwidth

Please provide sample code for the init and execution

Best Regards,

Ram

  • Hi Ram,

    Sorry for the delay. I believe there is work being done in order to support the requirement of having multiple RX and TX channels synchronized.

    Let me check internally on this and get back to you with what we can currently offer.

    In regards to your mode of operation for the AFE7950 is there one you already have created and tested in the AFE79xx Latte GUI?

    Best,

    Camilo