Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950
Tool/software:
Hi David,
According to the datasheet for the AFE7950, the maximum amplitude (power) that the AFE7950 device can tolerate is approximately 0 dBm at frequencies around 5 GHz, with an SFDR of approximately 78.5 dBc.
These parameters suggest that the total detectable dynamic range is around (+0 dBm to -78.5 dBm). This means that we should be able to detect signals and their frequencies within this range. Is this interpretation correct, or is there something I might have missed in these parameters?
I have also recorded some results on the AFE7950 EVM board, ranging from -2 dBm to approximately -55 dBm. The results obtained are as follows:
- ADC counts at -2 dBm: approximately ±11,800 counts
- ADC counts at -55 dBm: approximately ±30 counts
Given that our ADC has a 14-bit resolution and we achieve 16-bit resolution after DDC, is it possible to enhance the signal amplitude further beyond 0 dBm? This enhancement would allow the ADC counts to approach ±32,768.
Should my understanding is correct?
For Reference, I have attached some snapshots from the datasheet