Tool/software:
Hi
I use AF7954 and ZCU102.
I tried to program AFE but failed.
Below is the procedure I followed:
1. I run Latte( It seems to be called AFE79xx now )
2. Run setup.py (run->buffer)
3. Run devlnit.py (run->buffer)
4. Run ZCU102_4T_10Gbps.py (run->buffer)
5. Enter the following command.
logDumpInst.logFormat = 0x21
logDumpInst.rewriteFile = 1
logDumpInst.rewriteFileFormat4 = 1
device.optimizeWrites = 0
device.rawWriteLogEn = 1
6. Run ConfigAfe.py (run->buffer)
7. After completing step 6, I got an 'Afe79xxPg1Format5.txt'.
Afterwards, I tried to find SPI_convert.py to convert 'Afe79xxPg1Format5.txt' to spi, but I couldn't find it.
Can you tell me which directory SPI_convert.py is in?
And, is there an error in the script I'm using?
############## Read me ##############
#In HSDC Pro DAC tab, Select AFE79xx_2x2TX_44210; Data Rate = 491.52M
#In HSDC Pro ADC tab, Select AFE79xx_2x2RX_44210; Data Rate = 491.52M ---> To capture 4 RX channels
sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion
setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro
############## Top Level ##############
sysParams.FRef = 245.76
sysParams.FadcRx = 2949.12
sysParams.FadcFb = 2949.12
sysParams.Fdac = 2949.12*4
sysParams.externalClockRx=False
sysParams.externalClockTx=False
############## Digital Chain ##############
##### RX #####
sysParams.rxEnable = [False,False,False,False]
sysParams.ddcFactorRx = [12,12,12,12] #DDC decimation factor for RX A, B, C and D
sysParams.rxNco0 = [[9500,9500], #Band0, Band1 for RXA
[9500,9500], #Band0, Band1 for RXB
[9500,9500], #Band0, Band1 for RXC
[9500,9500]] #Band0, Band1 for RXD
##### FB #####
sysParams.fbEnable = [False,False]
sysParams.ddcFactorFb = [12,12] #DDC decimation factor for FB 1 and 2
sysParams.fbNco0 = [9500,9500] #Band0 for FB1 and FB2
##### TX #####
sysParams.ducFactorTx = [48,48,48,48] #DUC interpolation factor for TX A, B, C and D
sysParams.txNco0 = [[8071.875,8071.875], #Band0, Band1 for TXA
[8071.875,8071.875], #Band0, Band1 for TXB
[8071.875,8071.875], #Band0, Band1 for TXC
[8071.875,8071.875]] #Band0, Band1 for TXD
############## JESD ##############
##### ADC-JESD #####
sysParams.jesdSystemMode= [3,3]
#SystemMode 0: 2R1F-FDD ; rx1-rx2-fb -fb
#SystemMode 1: 1R1F-FDD ; rx -rx -fb -fb
#SystemMode 2: 2R-FDD ; rx1-rx1-rx2-rx2
#SystemMode 3: 1R ; rx -rx -rx -rx
#SystemMode 4: 1F ; fb -fb- fb -fb
#SystemMode 5: 1R1F-TDD ; rx/fb-rx/fb-rx/fb-rx/fb
sysParams.jesdTxProtocol= [0,0] # 0 - 8b/10b encoding; 2 - 64b/66b encoding
sysParams.LMFSHdRx = ["24410","24410","24410","24410"]
# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb = ["12410","12410"]
sysParams.rxJesdTxScr = [True,True,True,True]
sysParams.fbJesdTxScr = [True,True]
sysParams.rxJesdTxK = [16,16,16,16]
sysParams.fbJesdTxK = [16,16]
sysParams.serdesTxLanePolarity =[1,1,0,0,1,1,0,0]
sysParams.jesdTxLaneMux = [1,0,3,2,4,7,6,5] # Enter which lanes you want in each location.
# For example, if you want to exchange the first two lines of each 2T,
# this should be [[1,0,2,3],[5,4,6,7]]
##### DAC-JESD #####
sysParams.jesdRxProtocol= [0,0]
sysParams.LMFSHdTx = ["48410","48410","48410","48410"]
sysParams.serdesRxLanePolarity=[1,1,1,1,0,0,0,0]
sysParams.jesdRxLaneMux = [4, 7, 6, 5, 1, 3, 0, 2]#[1,0,3,2,4,6,7,5] # Enter which lanes you want in each location.
# For example, if you want to exchange the first two lines of each 2R
# this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd = [4, 4]
sysParams.jesdRxScr = [True,True,True,True]
sysParams.jesdRxK = [16,16,16,16]
##### JESD Common #####
sysParams.jesdABLvdsSync= False
sysParams.jesdCDLvdsSync= False
sysParams.syncLoopBack = True #JESD Sync signal is connected to FPGA
############## GPIO ##############
sysParams.gpioMapping = {
'H8': 'ADC_SYNC0',
'H7': 'DAC_SYNC0',
'N8': 'ADC_SYNC2',
'N7': 'ADC_SYNC3',
'H9': 'ADC_SYNC1',
'G9': 'DAC_SYNC1',
'N9': 'DAC_SYNC2',
'P9': 'DAC_SYNC3',
'P14': 'GLOBAL_PDN',
'K14': 'FBABTDD',
'R6': 'FBCDTDD',
'H15': ['TXATDD','TXBTDD'],
'V5': ['TXCTDD','TXDTDD'],
'E7': ['RXATDD','RXBTDD'],
'R15': ['RXCTDD','RXDTDD']}
############## LMK Params ##############
lmkParams.pllEn = True
lmkParams.inputClk = 10 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk = True
setupParams.fpgaRefClk = 122.88 # Should be equal to LaneRate/40 for TSW14J56
############## Logging ##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1.txt")
logDumpInst.logFormat=0x0 #Modify to 0x1 to save register scequence to log file. Script takes more time to execute.
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1
device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
setupParams.skipLmk = False
AFE.initializeConfig()
lmkParams.sysrefFreq = AFE.systemStatus.sysrefFreq
lmkParams.lmkPulseSysrefMode = False
AFE.LMK.lmkConfig()
Regards,
Jeongju Go