This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950-SP: REF CLK & SYSREF input level when the AFE is unpowered

Part Number: AFE7950-SP

Tool/software:

Hello

The Absolute maximum ratings specify SYSREF and REFCLK input voltage range of -0.3V - +1.4V .

I wish to make sure that this applies also to when the device is unpowered.

Regards,

Itai.