Tool/software:
When the TX_PLL of AFE7769 is set at 880MHz, a large power DC will be generated, and the QMC automatic calibration cannot go down, affecting the ACPR, this problem has a small probability, about 1/250, help to analyze what are the possibilities; In addition, is the library file version of AFE7769 still V2.20? Is there any update?