This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7921: AFE79xxEVM

Part Number: AFE7921

Tool/software:

HI,

    We are using AFE79xxEVM_ GUIv1p10_ Installer on our board  and we found the following problem, can  provide AFE79xxEVM_ GUIv1p9_ Installer software for comparison?

1.If 204B is set to 48410, an error will be reported when it is linked to the FPGA, and  24410 is OK,our FPGA 204B is set to 48410,but AFE7921 set to  48410 is can not link to my FPGA,and AFE7921 set to 24410 can link to my FPGA .   However, having someone else use our 48410 py script to run the configuration on the AFE79xxEVM_ GUIv1p9_ Installer will work fine.

2.The file size we generated with AFE79xxEVM_ GUIv1p10_ Installer is 395kb.   However, when I let someone else use our py script to generate 503kb, I found a lot more Information in comparison.

3.The configuration we generated using the AFE79xxEVM_ GUIv1p10_ Installer consumes 1.5W more power than someone else's configuration using AFE79xxEVM_ GUIv1p9_ Installer with  the same py script