Part Number: AFE7950
Tool/software:
What are the settings for "Transmitter ONLY MODE" and "Receiver ONLY MODE"?
How do I set it up?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AFE7950
Tool/software:
What are the settings for "Transmitter ONLY MODE" and "Receiver ONLY MODE"?
How do I set it up?
Hi,
Are you referring to fully disabling unused channels so that you could have Rx only or Tx only configs? Or do you mean to have all channels enabled but you would like to have Rx and Tx active at different times?
If it is the first one then you can fully disable channels using the enable parameters, sysParams.rxEnable/txEnable/fbEnable, in the Latte script.
If it is the second one then when the Tx or Rx is not needed then you can put them into a standby mode using the TDD pins (Either through controlling the GPIO pins or using registers to override the pin's state.
Regards,
David Chaparro