Part Number: AFE7950
Tool/software:
I have a question about the sampling rate of the AFE7950.
Are the combinations of sampling rate and interpolation/decimation only those in the following table in the datasheet?
(Table 8-5. RX Decimation Rates
Table 8-6. Interpolation Factors Between Input and DAC Sample Rates
Table 8-7. Decimation Factors Between FB ADC and Output Sample Rates)
For example, I was thinking of inputting a 2500MHz clock to the AFE, but looking at Table 8-6, the DAC SAMPLE RATE is 4500MSPS to 12000MSPS.
If I input a 2500MHz clock, do I need to increase the frequency to 5000MHz using the internal PLL to match Table 8-6?