Tool/software:
Hello,
We want to confirm a potential configuration for DAC38RF82 for our application.
We would like to output two I/Q streams from an FPGA, and they need to avoid overlap at the RF frequency.
Let's say we have two I/Q streams with a bandwidth of 100MHz, we need to space them at the output accordingly (side-by-side for example).
Paramaters:
- DAC Clock Frequency: 3300 MHz
- DAC Mode: Single DAC A
- IQ Pairs: 2
- JESD204 Lanes: 4
- Interpolation: 24x
- SERDES Rate: 2750MHz
RF Outputs:
- Output1: 1900 MHz [bandwidth: 1850-1950]
- Output2: 2100 MHz [bandwidth: 2050-2150]
Would the following setup work?
I am also concerned about the 3300MHz DAC clock which is too close to the 2GHz center frequency. Would this be a problem (by Nyquist terms or distortions)?
I cannot use 6600 MHz as the SERDES lane rate gets to 5500 MHz which is above the DAC limits?
Thanks in advance,
Ilias