Other Parts Discussed in Thread: TSW14J58EVM
Tool/software:
Hi,
The two devices are TSW14J58EVM and AFE7950EVM.
The current relevant settings are shown in the figure.
SysParams. FRef = 491.52
SysParams. FadcRx = 2949.12
SysParams. FadcFb = 2949.12
SysParams. Fdac = 2949.12 * 4
sysParams. DdcFactorRx = [12,12,12,12]
sysParams. DucFactorTx = [24,24,24,24]
The actual DAC sampling rate is 2949.12*4/24, and the ADC sampling rate is 2949.12/12, both of which do not reach the GHz level. What is the maximum sampling rate of this device? I hope to adjust the relevant parameter settings to maximize the actual sampling rate of both DAC and ADC.
In addition, I want to use the device to collect four channels of data at the same time, what command statement should I use?
Thank you very much!
All the best!
Jintao