Tool/software:
Hi Team,
As shown in the following figure, when the LMX8410L LO frequency is set to 11.75GHz, the IF I/Q port outputs normally, but why does the LO frequency in the GUI Mixer get a red alert message?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
As shown in the following figure, when the LMX8410L LO frequency is set to 11.75GHz, the IF I/Q port outputs normally, but why does the LO frequency in the GUI Mixer get a red alert message?
Hi Noel,
Two more question want to check with you. Please support. Thanks.
1. Why does the IF Port output in internal LO mode even if LO frequency is set at 11.75GHz?
Are there any relevant measurements to refer to?
2. operation In External LO mode, will LO port LO within the LMX8410L be used? Can LO frequency operate at 11.75GHz?
Hi Bo,
The mixer is specified to support a max. of 10GHz at both RF and LO port.
No matter if the LO is given externally or using the internal synthesizer, LO frequency has to be restricted to no higher than 10GHz.