Part Number: AFE8000
Tool/software:
Hi,
i went through the query in below link,
With AFE79xx series, NCO frequency can be dynamically changed within the same Nyquist zone only. (eg: If sampling freq is 3GHz and NCO1 is set to 1.3GHz then it is possible change dynamically only within the same nyquist i.e, 0.75 to 1.5GHz and cannot be set to other nyquist i.e,350MHz).
Does the same limitation apply to AFE8000 ?