This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950: Details functional description and default configuration of GPIO?

Part Number: AFE7950


Tool/software:

Hi, 

1. What is the functionality of GPIO pins ( Sleep , Alarm, BISTB0, BISTB1, SRDAMUX1, SRDAMUX2, INT1, INT2, Etc,,). Where I can refer the each pin functional description and configuration details?

2. What is the default configuration of each GPIO pins to be maintained? No details given in data sheet. Even if we can configured GPIO configuration through SPI, Power ON reset time what state to be maintained in Pull up/pull down externally.

3. In EVM Schematic AUXADC1, AUXADC4 is connected with SRDAMUX1 and SRDAMUX2. Is that any reason for connecting the corresponding pins ? Either any AUXADC1 can be connected to SRDAMUX?

4. What is the functional difference between RESETZ and TRESETZ pins? What is the default configuration for these pins.

5. Why ALARM1,ALARM2 is connected with INT1 and INT2?