This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7950EVM: AFE7950 GPIO Capabilities Beyond NCO Hopping?

Part Number: AFE7950EVM
Other Parts Discussed in Thread: AFE7950

Tool/software:

Hey,

I've been using the AFE7950 for NCO hopping across the 16 NCOs available in each channel, using the GPIO pins. I would like to know if there are any additional features or parameters, besides NCO hopping, that can be controlled using the GPIOs on the AFE.

Thanks in advance for any insights or suggestions!

LG

  • Hi LG,

    The AFE supports multiple functions and controls through the GPIO some of which are external DSA control, NCO hopping and Alarm reporting. Further description is available in the datasheet, section 'Low-Speed Digital I/O Configuration'. 

    Regards,

    David Chaparro