This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7769DEVM: Errors during Eval Kit Initialization using Latte GUI

Part Number: AFE7769DEVM
Other Parts Discussed in Thread: TSW14J58EVM

Tool/software:

Hi

I have an evaluation setup with AFE7769DEVM and TSW14J58EVM and I'm using Latte GUI to connect and configure the RF Transceiver. My PC has Windows 10 installed.

After running Latter application, I get the error "Couldn't Detect FPGA Reset FTDI. Please reset FPGA manually." in the small box down the window. I push SW3 on TSW board but it doesn't help. However, I read in a TI user guid that this can be ignored but I'd appreciate if there is any fix to this error.

Besides, when following TI quick user guide, after importing config spreadsheet and proceeding to initialization, a few errors comes up and the initialization does not complete without errors. In addition, during several same run, I get a few successful initialization which leads me to the fact that the errors are not consistent.

Below you can find the log during a test. Could you please help me to find the issue?

"

VI_ERROR_LIBRARY_NFOUND: A code library required by VISA could not be located or loaded.

Missing VISA Libraries: Only Dummy Instruments will be created.

Please install VISA Libraries for connecting to instruments.

Installation Information:

Keysight VISA Libraries: Keysight IO Libraries Suite 2024, Release Date: 25-March-2024, Build No.: 18.4.30319.0 .

Keysight IO Libraries Suite 2024 can be found in "Previous Versions" section from below link or by visting the Keysight website directly.

www.keysight.com/.../io-libraries-suite-downloads-2175637.html

AFE77xxDLibraryPG1p0

spi - USB Instrument created.

resetDevice

Kintex RegProgrammer - USB Instrument created.

Kintex RegProgrammer - USB Instrument created.

Kintex RegProgrammer - USB Instrument created.

Misc-B RegProgrammer - USB Instrument created.

Reset the FPGA and try again.

Loaded Libraries

FPGA Reset device not found

Reset the FPGA and try again.

FPGA Reset device not found

Refreshed GUI

Check if the MATLAB run-time 2021B 64-bit is installed.

Power Card - USB Instrument created.

#================ ERRORS:6, WARNINGS:1 ================#

#================ ERRORS:0, WARNINGS:0 ================#

Refreshed GUI

Device Initialization for ChipVersion: 1.0

2T2R1F Number: 0

Valid Configuration: True

laneRateRx: 9830.4

laneRateRx1: 9830.4

laneRateFb: 9830.4

laneRateTx0: 9830.4

laneRateTx1: 9830.4

2T2R1F Number: 1

Valid Configuration: True

laneRateRx: 9830.4

laneRateRx1: 9830.4

laneRateFb: 9830.4

laneRateTx0: 9830.4

laneRateTx1: 9830.4

DONOT_OPEN_Afe77xxDPG1p0_FULL - Device registers reset.

chipType: 0xa

chipId: 0x77d

chipVersion: 0x10

LMK Clock Divider - Device registers reset.

LMK Clock Divider - Device registers reset.

REFCLOCK is used from LMK source, ensure board connections are ok to do the same

LMK Configured.

Fuse farm load autoload done successful

No autload error

Fuse farm load autoload done successful

No autload error

AFE Reset Done.

pll1: True; LO Frequency: 2949.12

FPGA Reset device not found

FPGA Reset device not found

FPGA Configured.

AFE MCU Wake up done.

pll0: True; LO Frequency: 3500.0

pll1: True; LO Frequency: 2949.12

pll2: True; LO Frequency: 1900.0

AFE all PLLs configured.

AFE SerDes configured.

AFE Digital Chains configured.

AFE PAP configured.

AFE DAC Analog Writes configured.

AFE RX Analog Writes configured.

AFE FB Analog Writes configured.

AFE JESD configured.

AFE GPIO configured.

AFE TX IQMC-LOL Correction configuration Complete

AFE DPD Block configuration

AFE DPD Block configuration Complete

AFE RX IQMC configuration Complete

AFE RX AGC configuration Complete

AFE CFR configuration Complete

###########Device DAC JESD-RX 0 Link Status###########

Comma Align Lock Lane0: False; Please check if the transmitter is sending data and eye is good.

Comma Align Lock Lane1: False; Please check if the transmitter is sending data and eye is good.

CS State TX0: 0b00000000 . It is expected to be 0b00001010

FS State TX0: 0b00000000 . It is expected to be 0b00000101

Couldn't get the link up for device RX: 0

###################################

AFE Configuration Complete

#================ ERRORS:5, WARNINGS:0 ================#

"