Tool/software:
Based on MAX Current 4A, the Cout is on the datasheet (L: 6.8uH, 20.8 mΩ Cout: 2 x 47 μF + 22 μF).
Our design is designed to use up to MAX current 300mA (L: 10uH, 276mΩ Cout: 2 x 22 μF) and we need to make sure there is no problem.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Based on MAX Current 4A, the Cout is on the datasheet (L: 6.8uH, 20.8 mΩ Cout: 2 x 47 μF + 22 μF).
Our design is designed to use up to MAX current 300mA (L: 10uH, 276mΩ Cout: 2 x 22 μF) and we need to make sure there is no problem.

Hi Minkyu,
Can you provide more information on VIN and VOUT so can get better idea? Also please share a schematic of the application if you have one.
Thanks,
Dino
Hi Choi,
Does the customer have a spec for output voltage ripple?
Thanks,
Dino