Part Number: AFE7900EVM
Other Parts Discussed in Thread: AFE7900
Tool/software:
Hi ,
I’m currently testing the TI JESD204 IP on a Xilinx ZCU102 board connected to an AFE7900EVM.
To build the Vivado project, I used:
The ZCU102_AFE79xx_8b10b_10Gbps Latte script example
The reference design files from TI204C-IP-Release-v1.11-LATEST/reference_designs/zcu102_8b10b
The setup uses Vivado 2021.2 and TI JESD204C IP version 1.11.
To evaluate latency, I performed a loopback test by routing the JESD204 Rx input lane directly to the Tx output lane within the TI_204c_IP_ref.sv file, as shown below:
<modified code>
assign tx_lane_data = (enable_loopback) ? rx_lane_data : tx_lane_data_sine;
I applied a 5G, 100 MHz NR signal to the RxB input port (J1) and measured the corresponding delay at the TxB output port (J7).
The measured total latency is approximately 17.5 µs as shown below figure, which seems excessively high—even accounting for the digital filtering stages in the AFE7900 DDC/DUC paths.
Could you help me understand what might be contributing to this large latency during the loopback test?
My goal is to reduce the total latency to less than 1 µs.
Do you have any recommendations for optimizing latency when using the TI JESD204 IP with the AFE7900?
Any guidance or insights would be greatly appreciated.
Thank you!
-- Sangcheol